{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the part number for the replacement mushroom knob for the 9001 KR8, KR9, KR8P, KR9P, SKR8, SKR9, SKR8P, SKR9P?
Issue:
9001 screw-in replacement knob

Product Line:
Type K and SK Accessories

Environment:
30 mm Push Buttons

Resolution:
Unless noted otherwise, these are used on illuminated and non-illuminated devices:

Add suffix - 20 for 1and 3/8`` knob. Example: 9001KR9R20. This also works with other color knobs.
15/8`` Push-Pull Knobs for KR8, KR9, SKR8, SKR9 Operator:

Amber 9001A22
Black 9001B23 (color cap opaque and are for use on non-illuminated operator only)
Blue 9001L22
Clear 9001C22
Green 9001G22
Orange 9001S23 (color cap opaque and are for use on non-illuminated operator only)
Red 9001R22
Red* 9001R2205 *Marked Push Emergency Stop
White 9001W22
Yellow 9001Y22

Schneider Electric Canada