Search FAQs
Video: What is the difference between the HOM2150/HOM2200 and the HOM2150BB/HOM2200BB?
Issue:
Differentiating HOM2150/HOM2200 & HOM2150BB/HOM2200BB Circuit Breakers
Product Line:
Homeline Load centers
Resolution:
The older designed catalog numbers HOM2150 and HOM2200 were used as main breakers in the old obsolete Series 1 and 2 Homeline main breaker load centers. These main breakers are still used today in a few CSEDs (combination service entrance devices).
The HOM2150BB and HOM2200BB are designed ONLY to be used as branch breakers for use ONLY in the current Series S01 - S04 Homeline load centers rated 150 A max or higher.
NOTE: The HOM2150 and HOM2200 are NOT designed the same so they CANNOT be used as branch breakers and the current branch breakers, HOM2--BB, CANNOT be used as mains in the old obsolete panels.
Differentiating HOM2150/HOM2200 & HOM2150BB/HOM2200BB Circuit Breakers
Product Line:
Homeline Load centers
Resolution:
The older designed catalog numbers HOM2150 and HOM2200 were used as main breakers in the old obsolete Series 1 and 2 Homeline main breaker load centers. These main breakers are still used today in a few CSEDs (combination service entrance devices).
The HOM2150BB and HOM2200BB are designed ONLY to be used as branch breakers for use ONLY in the current Series S01 - S04 Homeline load centers rated 150 A max or higher.
NOTE: The HOM2150 and HOM2200 are NOT designed the same so they CANNOT be used as branch breakers and the current branch breakers, HOM2--BB, CANNOT be used as mains in the old obsolete panels.
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: