Search FAQs
What size fuse clips are provided in a 8538SC_12 or 8538SC_22?
Issue:
Identifying fuse clips in a size 1 combination starter
Product Line:
NEMA and Definite Purpose Contactors and Starters
Environment:
8538 Fusible Full Voltage Type (Class H Fuse Clips)
Cause:
Need to identifying the type of fuses required
Resolution:
30 amp 250 volt, will accept Class H, K or R fuses. If Class R only required, order rejection pin kit RFK03, the kit includes three fuse clip adapters which will reject all fuses accept Class R.
CTA-ID : 2022147
Identifying fuse clips in a size 1 combination starter
Product Line:
NEMA and Definite Purpose Contactors and Starters
Environment:
8538 Fusible Full Voltage Type (Class H Fuse Clips)
Cause:
Need to identifying the type of fuses required
Resolution:
30 amp 250 volt, will accept Class H, K or R fuses. If Class R only required, order rejection pin kit RFK03, the kit includes three fuse clip adapters which will reject all fuses accept Class R.
CTA-ID : 2022147
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: