{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are auxiliary contacts available for the Class 8903 Type LX* lighting contactors?
Issue:
Is there any auxiliary contact for lighting contactors type LX??

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
8903 type LX lighting contactors

Cause:
Auxiliary contacts part number needed for the 8903 type LX lighting contactors

Resolution:
All of the 8903 Type LX contactors are supplied as standard with 1 normally open and one normally closed auxiliary for customer use. These contacts are labeled 1A & 1B and are located on the mechanical latch attachment.

Schneider Electric Canada