{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

How do the contacts operate on a 9001KR8RH25, or SKR8RH25

Issue:
How is the configuration of contacts on a 9001KR8RH25?

Product Line:
Push Buttons and Operator Interface

Environment:
Class 9001 Type K

Resolution:
There are 2 contacts, 1-9001KA3, & 1-9001KA5. The KA3 is closed on Pull, but open on Neutral, and Push.
The KA5 is closed on Neutral, and Pull, but open on Push

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: