{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Will the GV2MC** and GV2MP** enclosures used with the GV2ME** manual starters accommodate auxiliary contacts and accessories?
Issue:
GV2M enclosure accessory

Product Line:
IEC Contactors and Starters

Environment:
GV2 Motor Starters and Protectors

Resolution:
GV2MC01, GV2MC02, GV2MP01 & GV2MP02 will accept (1) side mount auxiliary contact module mounted on either the left or right side as well as (1) of either front mount auxiliary contact or (1) voltage / shunt trip module. GV2MP03 and GV2MP04 will accept (1) side mount auxiliary contact module mounted on right side only as well as (1) of either front mount auxiliary contact or (1) voltage / shunt trip module.

Schneider Electric Canada