{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are there optional copper compression lugs available for J frame circuit breakers?
Issue:
Part number for copper compression lug kit for  J frame breakers.

Product Line:
Molded Case Circuit Breakers

Resolution:
Yes, there are 2 different lugs available. Catalog number CYA150JD is a set of 3 lugs with a wire range of (1) #4 to #2/0 AWG Cu per phase. Catalog number CYA250J3 is a set of 3 lugs with a wire range of (1) #2/0 to 300 kcmil Cu per phase.

Schneider Electric Canada