{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the contact blocks used with cover mounted operators in an XACA pendant station?
Issue:
Identify the part number of the contact blocks used for cover mounted operators in an  XACA pendant station

Product Line:
Harmony 22mm Pendant Stations

Environment:
Push Buttons and Operator Interface

Resolution:
ZB2BE101 is a spring return single speed normally open.
ZB2BE102 is a spring return single speed normally closed.
XENG1191 is a spring return two speed consisting of a normally open early closing and a normally open and normally closed.
XENG1491 is a spring return single speed consisting of a normally closed and 2 normally open.
XENG3781 is a latching, single speed consisting of a normally open interlocked with a second normally open. It is used with 2 adjacent push buttons.
XENG3791 is a latching, single speed consisting of a normally open interlocked with a normally closed. It is used with 2 adjacent push button.

Schneider Electric Canada