Search FAQs
Is the Class 2510 Type KR* or KW* available with conduit entry on top and bottom?
Issue:
Is the class 2510 Type KR* or KW* ( * indicates KR or KW followed by a 1, 2 5, or 6; the number may also be followed by A, B, or C.) available with conduit entry on top and bottom?
Product Line:
Manual switches
Environment:
Class 2510KR1, 2510KR2, 2510KW1, 2510KW1A, 2510KW1B, 2510KW2, 2510KW2B, 2510KW2C, 2510KW5, 2510KW5A, 2510KW5B, 2510KW6, 2510KW6B, 2510KW6C
Cause:
Top and bottom entry required
Resolution:
These switches are supplied as standard with one 3/4`` pipe tap in the bottom of the enclosure or the top if the enclosure box is reversed or flipped for top feed. To obtain the 3/4`` pipe tap in the top and bottom add suffix ``H`` to the part number. For example 2510KR1 becomes 2510KR1H, 2510KW1A becomes 2510KW1AH.
Is the class 2510 Type KR* or KW* ( * indicates KR or KW followed by a 1, 2 5, or 6; the number may also be followed by A, B, or C.) available with conduit entry on top and bottom?
Product Line:
Manual switches
Environment:
Class 2510KR1, 2510KR2, 2510KW1, 2510KW1A, 2510KW1B, 2510KW2, 2510KW2B, 2510KW2C, 2510KW5, 2510KW5A, 2510KW5B, 2510KW6, 2510KW6B, 2510KW6C
Cause:
Top and bottom entry required
Resolution:
These switches are supplied as standard with one 3/4`` pipe tap in the bottom of the enclosure or the top if the enclosure box is reversed or flipped for top feed. To obtain the 3/4`` pipe tap in the top and bottom add suffix ``H`` to the part number. For example 2510KR1 becomes 2510KR1H, 2510KW1A becomes 2510KW1AH.
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: