{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can you adjust the amperage or change the trip unit on a Powerpact breaker with an ET trip unit ?
Issue:
Adjust amperage or function on a breaker with an ET1.0I trip unit?

Product Line:
Circuit Breakers

Resolution:
ET trip units do not have an adjustable long time setting. It does have an adjustable instantaneous setting (1.5 - 12 x In). The trip unit is also not interchangeable or replaceable. If the long time setting needs to be adjusted, a new breaker with a trip unit of 3.0 or higher would need to be ordered.

Schneider Electric Canada