{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What are GV2L** or GV2LE** manual devices?

Issue:
GV2L** or GV2LE** description

Product Line:
IEC Contactors and Starters

Environment:
Tesys GV Manual Starter and Protectors

Resolution:
These devices are similar to the GV2 manual starters but provide magnetic protection only. The GV2L versions provide rotary style operators, where the GV2LE devices offer rocker lever operators. Basically these are magnetic circuit breakers and are typically are used ahead of a motor rated contactor and overload relay. However, they are not UL489 listed for use as circuit breakers in the United States.

Schneider Electric Canada