{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is the external operator available as a replacement part for the Class 2510 Type M*T** NEMA 7 & 9 cast aluminum enclosure?
Issue:
External operator replacement for the 2510 Type M*T** starters

Product Line:
NEMA Contactors and Starters

Environment:
2510 Type MT Manual Starters

Resolution:
Not from Square D / Schneider Electric. If the external operator is damaged there is also a possibility the integrity of the enclosure has been compromised. If the enclosure integrity is still in tact the replacement Handel operator can be obtained from Curlee manufacturing, Curlee enclosure part number is C8932.

Schneider Electric Canada