Search FAQs
What are the Acceptable wire sizes for Looping on the motor logic solid state overloads?
Issue:
What are the Acceptable wire sizes for Looping on the Class 9065 Type SSC10, SS010, SS110, SSC20, SS020, SS120 Solid State Overload Relays?
Product Line:
NEMA Contactors and Starters
Environment:
Class 8536/8736 Starters
Resolution:
Although looping is not recommended because it renders the dial setting to be incorrect they will accept #14 AWG to #8 AWG.
What are the Acceptable wire sizes for Looping on the Class 9065 Type SSC10, SS010, SS110, SSC20, SS020, SS120 Solid State Overload Relays?
Product Line:
NEMA Contactors and Starters
Environment:
Class 8536/8736 Starters
Resolution:
Although looping is not recommended because it renders the dial setting to be incorrect they will accept #14 AWG to #8 AWG.
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: