{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What component parts are included with the 9421 Type LN1 circuit breaker operating mechanism?
Issue:
Complete door mounted operating mechanism kit for the FAL, FHL, FCL circuit breakers

Product Line:
Type L Circuit Breaker Mechanism

Environment:
Class 9421 Type L door-mounted

Resolution:
The 9421LN1 consists of the following:
(1) 9421LF1 operating mechanism.
(1) 9421LH6 NEMA 1, 3R, 12 handle assembly.
(1) 9421LS8 standard (short) operating shaft.

Schneider Electric Canada