{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Are enclosures available for the GV2ME** manual starters?

Issue:
Separate enclosure GV2ME**

Product Line:
Tesys GV Manual Starter and Protectors

Environment:
North American Products

Resolution:
Yes, select from table below based on application. Please note, these enclosures will allow for 1 auxiliary accessory on right and left side.

Mounting Rating Part Number

Surface NEMA 1, IP 41 GV2MC01
Surface NEMA 12, IP 55 GV2MC02

Flush NEMA 1, IP 41 GV2MP01
Flush NEMA 12, IP 55 GV2MP02

Flush NEMA 1, IP 41 GV2MP03
Flush NEMA 12, IP 55 GV2MP04

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: