Search FAQs
What are the repair parts for an SC816D200C, series 002?
Issue:
Replacement parts for SC816D200C series 002
Product Line:
Combination Service Entrance Devices
Resolution:
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
The parts listed here are the only parts considered field repairable:
Replacement parts for SC816D200C series 002
Product Line:
Combination Service Entrance Devices
Resolution:
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
The parts listed here are the only parts considered field repairable:
- Rainproof Cap - 4056115803
- Rainproof Cap Mounting Screws - (2) 2142717161
- Meter Cover Assembly - 4056127952
- Meter Cover Mounting Screw - 4020513001K (contains 10 screws; only two are required)
- Utility Pullbox Cover - 4056133952 (includes cover latch)
- Load Center Cover Assembly - 4056128052 (includes hinges)
- Load Center Cover Mounting Rivet - (4) 2430315290
- Dead Front Interior Trim - 7329421701
- Dead Front Interior Trim Mounting Screw - 4020513001K (contains 10 screws; only one is required)
- Load Center Interior - 4056133352 (does not include main breaker or secondary main breaker mounting base; includes feed-thru lugs)
- Load Center Interior Mounting Screws - (7) 2153217161
- Main Breaker - HOM2200
- Main Breaker Retaining Hardware - 4056132701 (hold down strap that straddles across the main breaker), 4056152501 (clamp), 4056152601 (spacer), and 2159417721 (screw)
- Feed-Thru Phase Lug Assembly (Left) - 4056133252
- Feed-Thru Phase Lug Assembly (Right) - 4056133152
- Feed-Thru Phase Lug Assemblies Mounting Keps Nut - (2) 2342702000
- Feed-Thru Neutral/Ground Lug - 4025114550
- Feed-Thru Neutral/Ground Lug Mounting Nut - 2342702200
- Secondary Main Breaker Base Assembly- 4055841752
- Secondary Main Breaker Base Assembly Mounting Screws - 2153217161
- Meter Base Assembly - 4056149452 (includes load side meter jaws and load side lugs; does not include load side meter jaw blade guides)
- Meter Jaw - (2) 7329794850
- Meter Jaw Mounting Keps Nut - (2) 2342702001
- Meter Jaw Blade Guide - (4) 4052761901
Released for:Schneider Electric Canada
Explore more
Category:
Explore more
Category: