{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What handle operators are recommended for use with the Class 9422 Type R** flange mounted variable depth circuit breaker operating mechanisms?
Issue:
Handle operators for Variable-Depth Operating Mechanism

Product Line:
Molded Case Circuit Breakers

Environment:
Operating Mechanism for Circuit Breakers

Resolution:
Typically the Class 9422 Type A1 or A2 are recommended. However, if space is an issue then the Class 9422 Type A3 or A4 may be used.

Schneider Electric Canada