Search FAQs
What Handle Mechanisms can be Used with 400 amps 9422 Disconnect Switches?
Issue:
What Handle Mechanisms can be Used with Class 9422 Type TG1 or TG2 400 amp Flange Mounted Variable or Fixed Depth Disconnect Switches?
Product:
Operating Mechanisms and Disconnect Switches
Environment:
9422 Disconnect Switches
Resolution:
Use the 9422A5 or 9422A6 handle mechanism for fixed depths.
Use the 9422A7 or 9422A8 handle mechanism for adjustable depths.
The Types A1 thru A4 and A9 and A10 are not designed to operate this disconnect switch.
Note: Caution should be used selecting this switch and handle assembly because commercial enclosure manufactures do not make a standard enclosure which will accept the Type TG switches. Special enclosures must be ordered from the enclosure manufactures.
What Handle Mechanisms can be Used with Class 9422 Type TG1 or TG2 400 amp Flange Mounted Variable or Fixed Depth Disconnect Switches?
Product:
Operating Mechanisms and Disconnect Switches
Environment:
9422 Disconnect Switches
Resolution:
Use the 9422A5 or 9422A6 handle mechanism for fixed depths.
Use the 9422A7 or 9422A8 handle mechanism for adjustable depths.
The Types A1 thru A4 and A9 and A10 are not designed to operate this disconnect switch.
Note: Caution should be used selecting this switch and handle assembly because commercial enclosure manufactures do not make a standard enclosure which will accept the Type TG switches. Special enclosures must be ordered from the enclosure manufactures.
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: