{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the part number for the Handle Return Spring for the Class 9422 Type A1 and A2 handle assembly?
Issue:
Is there a replacement part number for the handle return spring for 9422A1 or 9422A2 handles?

Product Line:
Operating Mechanisms and Disconnect Switches

Environment:
Class 9422 Type A1 and A2 Handle

Resolution:
The Handle Return Spring part number is 30017-143-01.

Schneider Electric Canada

Explore more
Range:
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Product: