{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can a 9001B control station be wired directly to a motor, or does it need a starter?
Issue:
Are the 9001B control stations are motor rated?

Product Line:
Push Buttons

Environment:
9001B Control Stations

Resolution:
The contacts on the 9001B control stations are not rated for motor duty, they are only rated for control duty.

Schneider Electric Canada