{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the maximum horsepower capacity for a 9013FHG?
Issue:
9013FHG  Electrical Ratings

Product Line:
Pressure, Vacuum and Float Switches

Environment:
9013 Type FHG-Pumptrol Compressor Pressure Switch

Resolution:
9013FHG2,9,12,13,44 and 49
Single phase
115volts- 1.5HP
230 volts- 2HP

3- phase
115volts- 2HP
230 volts- 3HP
460/575 volts 1HP

DC
115volts- .25HP without FormM4
230 volts- .25HP ``

Control circuit rating
A600

9013FHG22 , 29 , 32, 53, 54, 59
Single phase
115volts- 2HP
230 volts- 3HP

3- phase
115volts- 3hp
230 volts- 5hp
460/575 volts 1hp

DC
115volts- 1/2HP (.25hp with Form M1 )
230 volts- 1/2HP ``

Control circuit rating
A600

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: