Issue:
Checking if the NEMA 12 enclosure of the 2510 type M can be converted to NEMA 3R for outdoor use.
Product Line:
2510M, 2510T Manual Starters
Environment:
NEMA Contactors and Starters
Resolution:
No, these enclosures are not dual rated NEMA 12/3R and therefore should not be used outdoors.
Checking if the NEMA 12 enclosure of the 2510 type M can be converted to NEMA 3R for outdoor use.
Product Line:
2510M, 2510T Manual Starters
Environment:
NEMA Contactors and Starters
Resolution:
No, these enclosures are not dual rated NEMA 12/3R and therefore should not be used outdoors.