{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does SqD make kits to expand the number of neutral terminals available on the neutral bar in an NQ or NF panelboard?
Issue:
Number of neutral terminals available on the neutral bar in an NQ or NF panelboard.

Product Line:
Panelboards.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
No additional retrofit neutral bars are available for NQ or NF type panels. The panel is designed to have as many neutrals as necessary for the number of branch circuits available.

Schneider Electric Canada