{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the solid neutral assembly for use in the J250F, J250S, J250R, J250AWK, J250DS, oand J250SS circuit breaker enclosures?
Issue:
Product design features

Product Line:
Circuit Breakers Enclosures

Resolution:
The solid neutral assemblies used in these enclosures is as follows:
1) For 15 - 100 A breakers use solid neutral catalog number SN100FA
2) For 110 - 250 A breakers use solid neutral catalog number SN400LA
NOTE: For 200% Neutral, amperage range 110 - 250 A, use SN400LA and use copper wire ONLY.

Schneider Electric Canada

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.