{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

MH-WP Panelboard Enclosures and Steel Gauge

Issue:
What gauge of steel are the MH-WP Nema 3R/12 enclosures made from?

Product Line:
Circuit Breaker panelboards and enclosures sold and supported in the USA.

Environment:
Enclosure steel gauge

Cause:
N/A

Resolution:
MH20WP through MH68WP - box, endwall and door is made of 14 gauge steel
MH71WP through MH86WP - box and endwall is 14 gauge steel and the door is 12 gauge steel

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: