{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the repair parts for a RC816F100CH Series M01?
Issue:
Current design repair parts

Product Line:
Combination Service Entrance Device

Environment:
Repair parts

Cause:
maintenance

Resolution:

NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
The parts listed here are the only parts considered field replaceable:
Meter Cover - 4056167850 (Includes latch)
Load Center Cover - 4056157550 (Includes hinges and latch)
Load Center Cover Mounting Screws - (4) 2159417121
Dead Front Interior Trim - 4056173401
Dead Front Interior Trim Mounting Screws - 4020513001K (This kit contains 10 screws. Only 2 screws are required to mount the interior trim)
Load Center Interior - 40561-619-50 (Does not include main breaker. Does include feed-thru lugs)
Load Center Interior Mounting Screws - (4) 2153217160
Main Breaker - QOM2100VH, Mounting Hardware - (2) 2342702001 Keps Nuts and (1) 4020511201 Screw
Meter Base Assembly - 4056190050 (Includes meter base, line side lugs, meter jaws, meter jaw blade guides and horn bypasses)
Meter Jaw - (4) 4052706950 (OBSOLETE - REPLACED BY 7329794850) (Line side meter jaws included in Meter Base Assembly)
Meter Jaw Mounting Keps Nuts - (4) 2342702001 (Line side meter jaw mounting keps nuts included in Meter Base Assembly)
Meter Jaw Blade Guide - (4) 4052761901 (Line side meter jaw blade guides included in Meter Base Assembly)
Line Side Horn Bypasses - (2) 4056150901 (Included in Meter Base Assembly)
Load Side Horn Bypass (Left) - 4052783101
Load Side Horn Bypass (Right) - 4052783102
Fifth Jaw Assembly - 4052797750
Fifth Jaw Assembly Mounting Screw - 2153217160
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: