{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What was the part number for an XB2 illuminated push-on / push-off operator?
Issue:
Part number for an XB2 illuminated push-on / push-off operator

Product Line:
Push Buttons and Operator Interface

Environment:
Harmony XB2 22mm Push buttons

Resolution:
*These products are now obsolete*
The XB2 product line used the standard illuminated operators and the ZB2BZ21 push on push off mechanism to obtain this functionality. The push-on / push-off functionality is obtained by adding the ZB2BZ21 mechanism between the operator and the contact block on any illuminated or non-illuminated push button.
See page 331 in Push Buttons and Operator Interface Specifier`s Guide, document 9001CT0001

Additionally, there are devices not commercialized in the US where the push-on / push-off mechanism was included in the operator. These operators began with the part number ZB2BH, followed by a color code. The same functionality is obtained by ordering the operator separately and the ZB2BZ21 mechanism instead.

Schneider Electric Canada