{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What size conductors will the lugs accept on the Class 9422 Type T__ 30 and 60 amp disconnect switch?
Issue:
What are the size conductors used with 9422T_ 30 and 60 amp disconnect switch (Lugs)?

Product Line:
Operating Mechanisms and Disconnect Switches

Environment:
Class 9422 Type T Disconnect switch

Resolution:
The standard switch supplied with aluminum lugs accommodates (1) #14 - #2 AWG aluminum or copper conductor per phase. If the switch is provided with factory modification Y157 then it is supplied with copper lugs which will accommodate (1) #14 - #4 AWG copper conductor per phase.

Schneider Electric Canada