{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is the Enclosure Cover-Only Available for Class 2510 Type MBG, TBG, MCG, or TCG NEMA 1 enclosed manual starters?
Issue:
Replacement cover-only needed as sometimes it gets defective or damage.

Product Line:
NEMA Contactors and Starters

Environment:
Manual Starters and Switches

Resolution:
No, suggest replacing the complete enclosure. Below is the list of NEMA 1, surface mount replacement enclosures.
Class and TypeSizeEnclosure Part Number
2510FAll9991EN1 *
2510KAll9991EN1 *
2510MM-0 & M-19991MG1 *
2510MM-1P9991MG2 *

* Discontinued

Schneider Electric Canada

Explore more
Range:
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Product: