{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the maximum current rating for the spade or quick connect terminals on the Class 8910 Type DP & Type DPA contactors?
Issue:
Max current rating of the spade or quick connect terminals on 8910DP & DPA contactors

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
Definite Purpose Contactors

Cause:
Identifying current ratings

Resolution:
30 amps, 75 degree Celsius conductor.

Schneider Electric Canada