Search FAQs
Can a 9007AW12 limit switch operate both in a CW and CCW directions ?
Issue:
How does a 9007AW12 operate?
Product Line:
Pressure and Limit SwitchesSquare D Class 9007 Limit Switches
Environment:
Square D Class 9007 Limit Switches
Resolution:
The 9007AW lever arm switches operate in the CCW direction as standard and can be field converted to operate in the CW direction . However they cannot operate in both directions at one time . If a switch is required to operate in both directions , consider a 9007C54B2
How does a 9007AW12 operate?
Product Line:
Pressure and Limit SwitchesSquare D Class 9007 Limit Switches
Environment:
Square D Class 9007 Limit Switches
Resolution:
The 9007AW lever arm switches operate in the CCW direction as standard and can be field converted to operate in the CW direction . However they cannot operate in both directions at one time . If a switch is required to operate in both directions , consider a 9007C54B2
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: