Search FAQs
Can I add programmable contacts to a Powerpact P or R frame breaker in the field?
Product Line:
Circuit Breakers
Resolution:
Yes. An externally mounted, field installable M2C kit for Powerpact P and R breakers is available. Cat # S64273.
NOTE: You need a BCM (breaker communications module) and P or H trip unit for the programmable contacts to work. BCM part number is S64205.
Circuit Breakers
Resolution:
Yes. An externally mounted, field installable M2C kit for Powerpact P and R breakers is available. Cat # S64273.
NOTE: You need a BCM (breaker communications module) and P or H trip unit for the programmable contacts to work. BCM part number is S64205.
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: