{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How do I access the dry contacts on the I-Line Integral TVSS unit?
I-Line Diagnostic Display PanelDanger label

The dry contacts are accessed by removing the dead front of the panel then the face plate of the TVSS. The I-Line series Surge Protective Device (SPD) is provided with dry contacts. The connection for the dry contacts (Exhibit C), is located and labeled on the back of the diagnostic display panel and will accept 22-14 AWG stranded or solid wire. The dry contacts are three-position, Form “C” type with Normally Open, Normally Closed and Common connections. The unpowered state shall be closed between terminals NC and COM. This is also the alarm condition. The opposite state, closed between terminals NO and COM, indicates that power is on to the unit and that no alarm condition exists. The contacts are designed for a maximum voltage of 24 Vdc / 24 Vac and a maximum current of 2 A.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: