{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Is there a direct mount handle available for the LK3____ non-fusible IEC style disconnect switches?

Issue:
What is the part number of the direct mount handle for the LK3 non-fusible IEC style disconnect switches?

Product Line:
Non-Fusible IEC style Disconnect Switches

Environment:
IEC Disconnect Switches

Resolution:
There is no need for a hole adapter kit in the likes of GS1 and GS2 as these switches are designed for through-the-door operation.

Schneider Electric Canada