{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How do you order Class 8910 Type DPA__ or Class 8911 Type DPS__ with a premium control coil?
Issue:
Identify the way to order a premium control coil for a DPA contactor.

Product Line:
Class 8910 Definite Purpose contactors

Environment:
Square D Contactors and Starters

Resolution:
Limited to 120 volt (voltage code V02) control coils only, add factory modification Y243 to the device part number, i.e. 8910DPA12V02Y243.

NOTE: Form Y243 is valid on Class 8910 Type DPA__, Type DPAG--__ contactors up to 63 amps and Class 8911 Type DPSO__, Type DPSG__ contactors up to 50 amps ONLY. There is no premium coil options for Class 8910 Type DP__ or Class 8911 Type DS__ compact contactors.

Schneider Electric Canada

Explore more
Range:
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Product: