Search FAQs
Does the class 9065 overloads comes with the standard normally closed control circuit contact?
Issue:
Do the 9065 overload come with the standard normally closed contact?
Product Line:
9065 Overload Relays
Environment:
NEMA and Definite Purpose Contactors and Starters
Cause:
Needs to confirm if the Square D overloads provided with the standard normally closed control circuit contact.
Resolution:
Yes, all class 9065 overloads are provided with the normally closed control circuit contact. Additionally, all three pole bimetallic overloads are also provided with non-isolated normally open alarm contact as standard.
Do the 9065 overload come with the standard normally closed contact?
Product Line:
9065 Overload Relays
Environment:
NEMA and Definite Purpose Contactors and Starters
Cause:
Needs to confirm if the Square D overloads provided with the standard normally closed control circuit contact.
Resolution:
Yes, all class 9065 overloads are provided with the normally closed control circuit contact. Additionally, all three pole bimetallic overloads are also provided with non-isolated normally open alarm contact as standard.
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: