Search FAQs
Are the Tesys LUB12 & LUB32 U-Line starter bases provided with auxiliary contacts?
Issue:
Does the Tesys LUB12 & LUB32 U-Line starter bases include the auxiliary contacts?
Product Line:
Contactors and Starters IEC
Environment:
North American Products
Product Line:
Tesys U Line Motor Starters
Resolution:
Yes, one normally and one normally closed contactor state auxiliary contact is included on the base. Additional auxiliary contacts can be added via the addition of one auxiliary contact module from the following list:
LUFN11 - One normally open , and one normally closed contact
LUFN20 - Two normally open contacts
LUFN02 - Two normally closed contacts
Does the Tesys LUB12 & LUB32 U-Line starter bases include the auxiliary contacts?
Product Line:
Contactors and Starters IEC
Environment:
North American Products
Product Line:
Tesys U Line Motor Starters
Resolution:
Yes, one normally and one normally closed contactor state auxiliary contact is included on the base. Additional auxiliary contacts can be added via the addition of one auxiliary contact module from the following list:
LUFN11 - One normally open , and one normally closed contact
LUFN20 - Two normally open contacts
LUFN02 - Two normally closed contacts
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: