{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Where is the fourth wire of a three phase, four wire NQ panelboard connected?

Issue:
Fourth wire connection of a three phase, four wire NQ panelboard connected.

Product Line:
Panelboards.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
The fourth wire should be connected to the neutral. To the the right and left of the incoming phase connections are neutral bars, and the incoming main neutral lug is mounted on one of them. The right and left neutral bars are bussed together; however, the bus connection may not be visible due to being covered by panel insulation. The ground bar, purchased separately, is mounted directly to the back plate of the panel enclosure.

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: