Search FAQs
Are the red rubber dropout pads for the 8502SE, 8536SE, 8502 SF or 8536SF devices available as replacement parts?
Issue:
Replacement red rubber dropout pads for the 8502SE, 8536SE, 8502 SF or 8536SF devices.
Product line:
NEMA 8502SE, 8536SE, 8502 SF or 8536SF Contactors and Starters
Environment:
Type S Contactors and Starters
Resolution:
Yes, the new pads are black in color, order (2) 31091-157-01.
Note: Approximate Date codes for the red bumpers installed in the NEMA Size 3 & 4 devices is 9509 through 9918.
Replacement red rubber dropout pads for the 8502SE, 8536SE, 8502 SF or 8536SF devices.
Product line:
NEMA 8502SE, 8536SE, 8502 SF or 8536SF Contactors and Starters
Environment:
Type S Contactors and Starters
Resolution:
Yes, the new pads are black in color, order (2) 31091-157-01.
Note: Approximate Date codes for the red bumpers installed in the NEMA Size 3 & 4 devices is 9509 through 9918.
Released for:Schneider Electric Canada
Explore more
Product:
Range:
Explore more
Product:
Range: