{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What does the Class 9422 Type ATF12 consist of?

Issue:
Class 9422 Type ATF12 description

Product Line:
Operating Mechanism & Disconnect Switches

Environment:
9422 ATF Disconnect switches

Resolution:
Consist of Class 9422 Type TF2 200 amp, fusible, variable depth, flange mounted disconnect switch and Class 9422 Type A1 operating handle. It is shipped assembled for right hand mounting but can be converted to left-hand flange mounting. The switch is rated 600VAC (250VDC using the two outer poles).

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: