Search FAQs
Is there an option for a manual remote reset for the Tesys U-Line?
Issue:
What is required for a manual remote reset option for the Tesys U-Line?
Product Line:
IEC Contactors and Starters
Environment:
TeSys U Motor Starter
Cause:
Needs to verify if there an option for a manual remote reset for the Tesys U-Line.
Resolution:
Yes, but requires the use of advanced control unit with the addition of the LUFDA10 function module wired to a normally open momentary pushbutton wired across X1 & X2.
What is required for a manual remote reset option for the Tesys U-Line?
Product Line:
IEC Contactors and Starters
Environment:
TeSys U Motor Starter
Cause:
Needs to verify if there an option for a manual remote reset for the Tesys U-Line.
Resolution:
Yes, but requires the use of advanced control unit with the addition of the LUFDA10 function module wired to a normally open momentary pushbutton wired across X1 & X2.
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: