{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the repair parts for the CH364DS, series F6 (may be shown as F06)?

Issue:
Current design repair parts

Product Line:
Heavy Duty Safety Switches

Resolution:
The repair parts for the CH364DS, series F6 (F06) are as follows. No other parts are available:
-Complete Line Base - 4056703450 (1 required; includes phenolic base, arc suppressors, lugs, rotor, switching blades, and fuse clips)
-Line Base mounting screws - 4020514202 (6 required per line base)
-Load Base Assembly - 4056677450 (1 required per phase; includes phenolic base, lugs, and fuse clips)
-Load Base mounting screws - 4020514202 (2 required per load base)
-Arc Suppressor Assembly - 4056677550 (1 required per phase)
-Arc Suppressor mounting screw - 4020514501
-Lug Assembly - 4025116251 (per lug)
-Lug Assembly mounting screw - 2140122240 (per lug)
-Switch Mechanism - 4056678650 (handle coupling, cover interlock defeat coupling, and lock plate gaskets may also need replacing)
-Handle Coupling - 4056699850
-Cover Interlock Defeat Coupling - 4056718850
-Switch Mechanism mounting screws- 2194918121 (2 required)
-Handle Assembly - 4056736850 (also recommend replacing lock plate gaskets)
-Lock plate - 4056738901 (also recommend replacing lock plate gaskets)
-Lock plate Gasket - 4050322802 (2 required) - Obsolete. Replaced with 4050322803
-Lock plate mounting screws - 2194918121 (2 required)
-Ground Lug - 4025101851 (2 required)
-Ground Lug Mounting Screw - 4020514801

Schneider Electric Canada

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: