{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the torque requirement for Type B melting alloy style overload thermal units used with Class 8536 Type SA_, SB_, SC_, SD starters?
Issue:
What is the torque requirement for Type B thermal units used with Class 8536 Type SA_, SB_, SC_, SD starters or Class 9065 size 1 or size 2 separate mount overload relays?

Product Line:
NEMA Contactors and Starters

Environment:
Class 8536 Type SA_, SB_, SC_, SD starters or Class 9065

Resolution:
18 to 21 inch pounds.

Schneider Electric Canada