{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What size of control wire should be used to connect a shunt trip for the H, J, and L frame breakers?
Issue:
What size of control wire should be used to connect a shunt trip for the H, J and L frame breaker?

Product Line:
Powerpact H, J and L frame

Resolution:
Each terminal may be connected by one 18–14 AWG (1.0–2.5 mm²) stranded copper wire. Terminals used should be C1 and C2.

Schneider Electric Canada