{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What are the main differences between the melting alloy and Motor Logic solid state overload relays?
Issue:
What is a melting alloy overload and what is a motor logic solid state overload?

Product Line:
NEMA style Overload Relays

Environment:
North American Products

Resolution:
The melting alloy type overload relays require the selection of thermal units, have relatively tight trip current ranges, are ambient sensitive and provide manual reset only. The Motor Logic solid state overload relays offer adjustable trip current ranges without the requirement of thermal unit selection, provide adjustable 3:1 trip current ranges, phase loss phase imbalance protection and Class II ground fault detection (Feature Base Only). The Motor Logic overloads also are ambient insensitive and are supplied with a sealable cover over the trip current adjustment dial.


 

Schneider Electric Canada

Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.