{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the kVA ratings for Square D High Efficiency dry type Transformers?
Issue:
Transformer kVA sizes

Product Line:
LV Transformers

Environment:
Applies to Low Voltage Transformers by SquareD/Schneider Electric

Cause:
Transformer sizing for different applications.
Resolution:


Square D Transformers meet the efficiency requirements of DOE 2106 in 3 phase 15 kVA through 750 kVA and 1 phase 15 kVA through 333 kVA


Schneider Electric Canada