{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are the Class 8903 Type PB__ lighting contactors available with 600 volt control coils?
Issue:
Are 600V Coils available with the Class 8903 Type PB Lighting Contactors?

Product Line:
NEMA Contactors and Starters

Environment:
8903 Type PB Lighting Contactors

Resolution:
No, 480Vac maximum

Schneider Electric Canada

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.