{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the AL1200P6KU lug kit be used on the I-Line version of the PowerPacT M and P frame circuit breakers?
Issue:
Need to use (3) 600 kcmil wires

Product Line:
Circuit Breakers

Resolution:
No, the AL1200P6KU lug is NOT for I-line breakers. It is certified only for unit mount breakers. The reasons includes wire bending space in I-Line panels, as well as electrical and mechanical interference with the I-Line mounting bracket, and lack of UL approval. For wire sizes/numbers that are not supported by the P frame, you can use the R frame, which will take up to (4) 600 kcmil wires per phase.

Schneider Electric Canada