{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is the 2510KR1H a factory sealed device?
Issue:
Are NEMA 7&9 Manual switches factory sealed?

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
2510 type KR NEMA 7 9 & 3R manual switches

Resolution:
This is an explosion proof cast aluminum enclosed manual switch rated NEMA Type 3R, 7 and 9. It is intended for use with Class 1 Groups B, C, D or Class 2 Groups E, F, G; Division 1 & 2 applications. This is not a factory-sealed device and therefore can be disassembled in order to replace the open style switch or other internal components.

Schneider Electric Canada

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: