{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Can Arc Fault Breakers (Like HOM-CAFI, QO-CAFI and HOM-DF, QO-DF) and Ground Fault Breakers(HOM-GFI and QO-GFI) be used in a Combination Service Entrance Devices?

Issue:
Product Design Features

Product Line:
Combination Service Entrance Device (CSED)

Environment:
Branch Breakers

Issue:
Application

Resolution:
Yes, the Arc Fault branch breakers, Dual Function(combined CAFI and GFI) and Ground Fault branch breakers can be used in the appropriate CSED.
NOTE: The Homeline branch breakers can ONLY be used in the CSED that accept Homeline and the QO branch breakers can ONLY be used in the CSED that accept QO.



Schneider Electric Canada